Other Parts Discussed in Thread: TLV320AIC33
Hi,
I am working on DM6446 DVEVM board.
In the guidelines document, I found the following statements
The McBSP’s DX pin on the DM644x can be configured to operate as a SPDIF
transmitter. The DM644x EVM supports a single SPDIF output with both analog and
optical interfaces. The analog SPDIF output pin is routed to a level translator then to a
driver and filter circuit before being output on J13. The same level translator is used for
another driver which then drives the optical transmitter U65. When the SPDIF interface
is enabled the TLV320AIC33 codec is disabled.
Presently, my SPDIF interface is enabled, but I cant find any guidelines to disable it and thereby enable my codec.
Can anyone guide me in this case?
Thanks and Regards,
Sidharth