This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/66AK2H12: linux matrix run failure!

Part Number: 66AK2H12


Tool/software: Linux

hi.

i used 2 boards. k2h and custom board similar to k2h. i burn ti-u-boot and linux kernel (PROCESSOR-SDK-LINUX-K2HK  04_02_00_09) on both of them.

http://git.ti.com/ti-u-boot/ti-u-boot 

http://software-dl.ti.com/processor-sdk-linux/esd/K2HK/latest/exports/ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin 

kernel boot on 2 boards and kernel reports on both of them are similar. but Matrix did not run in any boards.

(i tried MCSDK 3.01.04.07 prebuild image on k2h and matrix ran)

Serdes and lans are configured on both and i have ping in both of them. i read this page

http://processors.wiki.ti.com/index.php/Matrix_Users_Guide  

and used these commands:

/etc/init.d/matrix-gui-2.0 stop
/etc/init.d/matrix-gui-2.0 start

but matrix doesnt work. why matrix doesnt run on windows browser?