Tool/software: Linux
Hello,
I am trying to overlay PNG images and text messege in real-time video stream, I'm testing with the following pipeline
gst-launch-1.0 -v v4l2src device=/dev/video1 num-buffers=5000 io-mode=4 ! \ 'video/x-raw, format=(string)YUY2, width=(int)1920, height=(int)1080' ! \ vpe num-input-buffers=8 ! queue ! \ textoverlay text="TEXT1:ABC" halignment=4 valignment=3 deltax=100 deltay=100 ! \ gdkpixbufoverlay location=test.png offset-x=200 offset-y=200 overlay-width=240 overlay-height=320 alpha=0.8 ! \ waylandsink
The pipeline is running successfully .However, the CPU usage is about 115% and video frame rate dropped significantly.
I wonder if I missing some caps, or what can I do to resolve the issue,like using GPU?
Thanks,
Lex