This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5726: DDR data line swapping

Part Number: AM5726

Hi,

I have qestion about DDR3 data line swap of AM572x.
I am planning to use two 16-bit DDR3 memories for one DDR I / F of AM572x as the EVM.

In the case of the EVM as shown below, DQS0 and DQS1 are connected to one DDR3 memory, and DQS2 and DQS3 are connected to the other DDR3 memory.



Is it possible to swap DQS 1 and DQS 3 as shown below? Of course, D8-D15 and D24-D31 are also swapped.

Best regards,
H.U