This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beginning Assembly Language ... !

Hey,

I have done C programming for C6000 DSP, can anyone help where i can start for Assembly language Programming ?

Regards

Saad Shuja.

 

 

  • Hi,

    This wud be a good starting point.

    http://jason.sdsu.edu/c6x/ASSEMBLE.PDF

    Regards,

    Sid

  • Saad Shuja said:

    I have done C programming for C6000 DSP, can anyone help where i can start for Assembly language Programming ?

    just curiosity... why do you want to programm in assembler? or better - what part in your application requires the use of assembler? if its optimization... it will be quite hard to beat the TI compiler/optimizer from my point of view

  • Thomas, yes its for optimization. Hey i wanna test the following code written in Assembly

              .def _envelope
    _envelope:.cproc    input,prev_in,output,npts
              .reg      i,curr_abs,prev_abs,sign,CONST
              .reg      x,input1,output1,output2
              .reg      C1_Q14,C2_Q14
              MVK       -15415,C2_Q14
              MVK       31565,C1_Q14
              ABS       prev_in,prev_abs
              ZERO      i
    LOOP1:    LDH       *input++,input1
              LDH       *--output,output1
              LDH       *--output,output2
              ADD       output,4,output
              ABS       input1,curr_abs
              SUB       curr_abs,prev_abs,x
              SSHL      x,16,x
              SHR       x,5,x
              SMPY      output1,C1_Q14,output1
              SMPY      output2,C2_Q14,output2
              SADD      x,output1,x
              SADD      x,output2,x
              SSHL      x,1,x
              MVK       -32768,CONST
              MVKH      0x00008000,CONST
              SADD      x,CONST,x
              SHR       x,16,x
              STH       x,*output++
              MV        curr_abs,prev_abs
              ADD       i,1,i
              CMPLT     i,npts,sign
        [sign]B         LOOP1
             
              .return
              .endproc

    how can i test it. The question is how can i call this function from a C function call. Because when i try to compile it, all variables defined in this routine show that they are undefined.

  • Hi...

    well - as I said, its just curiosity. I try to avoid assembler if possible (and as I said before - I find it more or less impossible to beat the TI optimizer with hand-tuned inline assembler code). The only inline assembler instruction I like is " nop " ;-)

    Did you use the possibilities of pragmas and optimizer switches already? You have a loop and porbably can get a lot of performance if you give details of the loop using #pragma MUST_ITERATE

    bye,

    Thomas