Part Number: AM3352
Other Parts Discussed in Thread: TLV320AIC33, AM3358,
Tool/software: Linux
Hi,
I am trying to make an 8 slot tdm rx/tx with mcasp. We are going to connect a fpga, so we don't need a codec. Below shows my dts file. I used a dummy codec but i was not able to get the davince-mcasp.c file to print out any logs. It appears that the dummy codec doesn't make the connection to the mcasp drivers. Any ideas why the connection is missing?
codec_test: codec_test {
compatible = "linux,snd-soc-dummy";
#sound-dai-cells = <0>;
status="okay";
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "AM335x-TDM";
// simple-audio-card,format = "dsp_a";
simple-audio-card,format = "dsp_b";
// simple-audio-card,format = "i2c";
simple-audio-card,frame-master = <&sound_master>;
simple-audio-card,bitclock-master = <&sound_master>;
// simple-audio-card,bitclock-inversion;
// system-clock-frequency = <24000000>;
// system-clock-direction = "out";
status="okay";
sound_master: simple-audio-card,cpu {
sound-dai = <&mcasp0>;
system-clock-frequency = <24000000>;
system-clock-direction = "out";
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <16>;
};
sound_master1: simple-audio-card,codec {
// sound-dai = <&tlv320aic3x>;
sound-dai = <&codec_test>;
};
};
mcasp0_pins: mcasp0_pins {
pinctrl-single,pins = < /**/
0x120 ( PIN_INPUT_PULLDOWN | MUX_MODE6 ) /* (N18) gmii1_txd2.mcasp0_ahclkx */
0x12c ( PIN_INPUT_PULLDOWN | MUX_MODE6 ) /* (N19) gmii1_txclk.mcasp0_aclkx */
0x130 ( PIN_INPUT_PULLDOWN | MUX_MODE6 ) /* (M19) gmii1_rxclk.mcasp0_fsx */
0x134 ( PIN_OUTPUT_PULLDOWN | MUX_MODE6 ) /* (N17) gmii1_col.mcasp0_axr0 */
0x138 ( PIN_INPUT_PULLDOWN | MUX_MODE6 ) /* (N16) gmii1_rxd0.mcasp0_axr1 */
>;
&i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
clock-frequency = <100000>;
status = "okay";
tlv320aic3x: tlv320aic3x@1b {
compatible = "ti,tlv320aic3x";
reg = <0x1b>;
#sound-dai-cells = <0>;
status = "okay";
};
/* tlv320aic33: tlv320aic33@1b {
compatible = "ti,tlv320aic33";
reg = <0x1b>;
#sound-dai-cells = <0>;
status = "okay";
}; */
};
&mcasp0 {
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&mcasp0_pins>;
status = "okay";
op-mode = <0>; /* 0: MCASP_IIS_MODE, 1: DIT */
tdm-slots = <8>;
/* 4 serializers */
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
1 2 0 0 /* AXR0 AXR1 AXR2 AXR3 */
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
Rob