This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to work with MMC 4bit mode in wince6.0



Hi All,

I'm facing a problem in using MMC for booting for 4/8 bit mode. I can use sd card in 4bit mode and 24Mhz but in the mmc it working only in 1 bit.

Can any one suggest an idea how boot from mmc card using  4/8bit?

The messages which i got from debug port is mentioned below.

Init HW: controller RST
SDHC: 1 bit mode
SDCARD: reqested speed 1000000, actual speed 1000000
SDHC: command response timeout CTO!
MMC::MMCCommandResponse: MMCSendCommand error, command = 8
MMC::MMCCommandResponse: Command Response Error
SDHC: command response timeout CTO!
MMC::MMCCommandResponse: MMCSendCommand error, command = 55
MMC::MMCCommandResponse: Command Response Error
SDCARD: reqested speed 25000000, actual speed 24000000

Thanks in Advance

Jethin