Part Number: AM5K2E02
Our customer is looking into the use of the AM5K2E02 Dual Core ARM KeyStone II System-on-Chip (SoC) processor in an application where one of the cores would be disabled.
Having read through the datasheet I notice the following warning.
“10.2.1.3 Prolonged Resets
Holding the device in POR, RESETFULL, or RESET for long periods of time may affect the long-term
reliability of the part (due to an elevated voltage condition that can stress the part). The device should not
be held in a reset for times exceeding one hour at a time and no more than 5% of the total lifetime for
which the device is powered-up. Exceeding these limits will cause a gradual reduction in the reliability of
the part. This can be avoided by allowing the device to boot and then configuring it to enter a hibernation
state soon after power is applied. This will satisfy the reset requirement while limiting the power
consumption of the device.”
I would be grateful if you could obtain answers to the following questions:
-
In relation to the above warning, are there any similar effects on the reliability of the device if one core is disabled?
-
Are there any Application Notes or User Guides that describe methods of how to disable one of the ARM cores ?