This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: PCIe EP issues with Windows7 PC

Part Number: AM5728

Tool/software: Linux

Hi everyone,

Now, I use the am5728-evm board. It works as EP mode, I insert it in widows 7 PC , the PC scan the am5728-evm board as unkown PCIE device. Then I generate a PCIE driver with windirver, after install the PCIE driver nomally , it displays that the device can not find enough resources to use (Code 12), the same error code as CY.
I download the linux evm sdk version the same as "training.ti.com/am57x-pcie-ep-demo-processor-sdk-linux displays. The version is "ti-processor-sdk-linux-am57xx-evm-03.02.00.05-Linux-x86-Install.bin" , "software-dl.ti.com/.../index_FDS.html", the am5728-evm board kernel configs as "processors.wiki.ti.com/.../Linux_Core_PCIe_EP_User's_Guide" .
How can I confirm the am5728-evm board works ok? If it works normal , how can I use the PCIE device in ep mode, if there is any example program ? If I need to change any configeration to make the PC driver works normal , please teach me .

Thank you !!!