Does anyone know if there is a graphics library for the DM6437 that can be linked with Dsp/Bios?
Thanks, Wing.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does anyone know if there is a graphics library for the DM6437 that can be linked with Dsp/Bios?
Thanks, Wing.
Is this what you looking for? http://focus.ti.com/lit/ml/sprt502a/sprt502a.pdf
If not, what type of application are you having in mind?
Looks like eVRU may be the vector rendering engine that works with the OSD of the DM6437. I will contact them as to what user interface objects are available with their package or may be they have a user interface add-on library for eVRU. Thanks.
I believe they do have user interface library GUiliani available in addition to eVRU.
http://tes-dst.com/tes-dst/technology-a-ip/user-interface.html
In addition, our customers have also created number of bitmap images of menu/UI layout and they move from one bitmap to another when UI selection is done. This can only be done if the menu is quite static and can be represented using finite number of bitmap images.
Prateek