Part Number: AM5728
Posting on behalf of the field team.
Attempting to start CCS based evaluation for PRU on AM572x GPEVM - running into issues with JTAG connection.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Posting on behalf of the field team.
Attempting to start CCS based evaluation for PRU on AM572x GPEVM - running into issues with JTAG connection.
Good reference is the following wiki
http://processors.wiki.ti.com/index.php/AM572x_GP_EVM_Hardware_Setup#Powering_up_the_EVM
Here are the recommended steps to connect
- Connect the XDS200 to the GPEVM and to the host PC.
- Connect the serial port cable to the host PC
- Open a terminal and configure it to the serial port defined by the cable
- Insert the SD card into the GPEVM slot with a valid U-boot
- Plug the power jack to the GPEVM and press the S1 button to turn it on
- At the terminal, halt the u-boot procedure to keep the board powered
- Open CCS, create a target configuration file that uses the Connection as Texas Instruments XDS2xx USB Debug Probe and the Board or Device as either GPEVM_AM572X or GPEVM_AM572X_SiRevA (if using older silicon)
- With the target configuration file in focus, click on the green bug button to Launch a project less debug session
- Once at the debug session opened, highlight the Texas instruments XDS2xx USB Debug Probe/CortexA15_0 and hit Ctrl+Alt+C to connect to this core
- Go to menu Scripts and select AM572X Multicore Initialization AM572X_Multicore_EnableAllCores
- Highlight other cores and hit Ctrl+Alt+C to connect to each of them.
o Important: the significant difference between Si Rev 1.x and Rev 2.x is the JTAG mapping of the ICSS – if you can’t connect to the PRUs, change the Device to the other Si rev.
By doing this we were able to connect to most of the cores, including the offending ARM9_ICONT1
The error message typically shows up if you don’t release the core from reset. More details on :
http://processors.wiki.ti.com/index.php/GSG:Connecting_to_slave_cores_in_SoC_devices_v5
Biser-san, Mukul-san, All,
Thank you for your support.
I can Launch am572x, and I can connect A15 core.
But I cannot connect PUR
Could you please let me know how do I connect PRU.
I did try to chang the Device to the other Si rev.
My CCS are Version: 6.2.0.00050 and Version: 7.4.0.00015.
Regards,
Shinji Ueda