Part Number: AM5728
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hello.
I'm using am5728 and the dsp1,dsp2 load on linux.
I'm use
pdk : 1.0.7
ipc : 3.46.0.2
bios : 6.46.5.55
psdk : 4.0.0.4
For dsp2 of am5728 device I'm trying to add the timer of the sysbios.
I Add In dsp2 .cfg file the timer.
| var Clock = xdc.useModule('ti.sysbios.knl.Clock'); Clock.tickPeriod = 100; Clock.tickSource = Clock.TickSource_USER; var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
Timer.checkFrequency = false; timerParams.tiocpCfg.softreset = 0x0; timerParams.tiocpCfg.idlemode = 0x3; timerParams.twer.ovf_wup_ena = 0x1; |
after linux boot is completed(without dsp2 firmware), menually loading dsp2 firmware, and Timer was work very well.
"echo 41000000.dsp > /sys/bus/platform/drivers/omap-rproc/bind"
The problem is, that copy the dsp2 firmware "/lib/firmware/dra7-dsp2-fw.xe66" and reboot.
When the dsp2 firmware is loaded, a kernel panic occurs, which is caused by the presence of Timer.create() function in .cfg file.
Please check if the Dsp2.cfg file is wrong.