This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about cmem module on kernel 2.6.30



All,

 

I am using the newest kernel (2.6.30) on DM355. I need to use cmem module from LSP 1.20 package. When I recompiled cmem module using kernel 2.6.30, It seemed it can not get work. (kernel was dead). I don’t why it is. How to use cmem module for new kernel 2.6.30? Thanks very much.

 

BR,

Jeff

  • Modules like CMEM are only thoroughly tested with the kernel of the DVSDK that they are packaged with, it is possible that there are some incompatibilities between the CMEM you are using and the 2.6.30 kernel. The CMEM module from LSP 1.20 is rather old, you may want to try a newer DVSDK or LSP, though there is no guarantee that it will build and function properly with newer kernels.