Part Number: AM3352
Tool/software: Linux
Hello,
I'm working on a custom board based on Sitara AM3352, with Linux-RT 4.4.19.
I have a Modem connected via USB interface, and when the PPP crash, my application turn off and on the modem.
In this situation the entire system slow-down an I need to reboot.
//-------------------------------------------------------------
cat /proc/loadavg
18.50 8.84 3.81 2/117 31510
//-------------------------------------------------------------
Turning off the modem, removes the USB interface used by PPP connection, and it seems to create this problem.
Could you give me any advice?
Regards,
Luigi