This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: C6678 SRIO Gen 1 vs Gen 2 throughput

Part Number: TMS320C6678

 I would like to know the effective bandwidth of SRIO Gen 1 and Gen 2. , not  the bitrate difference of SRIO Gen 1 and Gen 2

I found that there are number of doc. talk about throughtput

Throughput Performance Guide for KeyStone II Devices

http://www.ti.com/lit/an/sprabk5b/sprabk5b.pdf

Throughput Performance Guide for TCI66x KeyStone Devices

http://www.ti.com/lit/an/sprabh2a/sprabh2a.pdf

Throughput Performance Guide for C66x KeyStone Devices

e2echina.ti.com/.../Throughput-Performance-Guide-for-C66x-KeyStone-Devices-_2800_Rev.-A_2900_.pdf

And the SRIO througthput data is different ,

C6678, 1GHz is used , which is one is suitable for reference. 

And what is SRIO data read latency in SL2, DDR3 in different playload size?

Thanks.

Stephen