This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Qt warning

Part Number: AM5728

Tool/software: Linux

Hi,

I have compiled qt-everywhere-opensource-src-5.7.1 with ti-processor-sdk-linux-am57xx-evm-04.02.00.09 SDK.

The compiled qt5.7 is installed in ~/ti-processor-sdk-linux-am57xx-evm-04.02.00.09/targetNFS/usr/local/Qt5.7.1_opengl/

i have reffered http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_QT I  downloaded qt-opensource-linux-x64-5.7.0.run installed the same.

Even though the steps are mentioned for AM335x i have followed the same since both AM335x & AM5728 are from Sitara Family.

I am getting warning like Device type is not supported by Qt version. If I will select Device Type as "Generic Linux Device" ,then I am not getting any drop down option for "Device".Thats why i have selected Desktop as Device Type. Let me know the reason for the same.

Regards,

Biswajit