Part Number: TDA3LA
Tool/software: Code Composer Studio
Hi!
I have an application with a TDA3LADBABFRQ1.
I am using Code Composer v7.2.0.00013
The debugger in use is a Spectrum Digital XDS560v2 STM
I'd like to utilize the functionality of the STM to trace various information from the TDA3.
The ultimate goal would be to use the CToolsLib to write different debugging information into the debugger and analyze them on the computer.
But first things first:
My understanding is, that if I select the following menu:
I would get a possibility to set up the system trace connection to the TDA3
I use these settings to get the trace data from the TDA3:
It then tells me, I need a gel script
I found these in the installation folder of code composer:
c:\ti7\ccsv7\ccs_base\emulation\gel\TDA3x\
So I load them into CCS.
It turns out that the script Enable_ETB_For_STM() does not work. (This by the way also a point of confusion, because the script actually seems to try to activate ETB, even though I want to use STM to trace out the data, and not the ETB as a circular storage)
It throws this error message:
Enable_ETB_For_STM() cannot be evaluated. invalid page: data at (int *) 0xD4164FB0@data [TDA3xx_stm.gel:64] at Enable_ETB_For_STM()
The @data keyword seems to be the trouble. Nevertheless, I am not even sure if that address would be even correct. If I open that in the memory browser, it tells me there is nothing.
Shouldn't it be rather the address: 0x54164000
As from the datasheet I see:
So my question would be. Am I on the right track to get STM working.
If yes, can TI provide me with the correct set of gel files. I have checked the latest CCS v8.0.0.00016 , but it has basically the same gel files.
What be even more smashing, if someone could verify on their side with a similar setup, if what I am trying to do does work.
I have added the gel files which were in my CCS installation, and the ccxml that I use to init the debugger.