Other Parts Discussed in Thread: AM5728
Tool/software: Linux
Dear team,
I am running decode on am5718.The board is a custom designed.
When the board booting or reload firmware,the ipu2 can not work.
here is error message.Some message is added by myself.
[ 162.199528] remoteproc remoteproc1: stopped remote processor 55020000.ipu
[ 162.209673] remoteproc remoteproc1: releasing 55020000.ipu
[ 162.221112] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 162.229890] remoteproc remoteproc1: 55020000.ipu is available
[ 162.246253] remoteproc remoteproc1: powering up 55020000.ipu
[[ 162.259223] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3743164
[ 162.269124] omap-iommu 55082000.mmu: deassert_hardreset
[ 162.274394] in 2 2 1 700 210 214
[ 162.277635] stat 7
[ 162.279656] in1 2 2 1 700 210 214
[ 162.283186] stat 7
[ 162.285204] out 2 2 1 700 210 214
[ 162.288564] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 162.298398] rproc_fw_boot 1124
[ 162.303116] rproc_fw_boot 1128
[ 162.306187] rproc_fw_boot 1136
[ 162.332614] rproc_fw_boot 1159
[ 162.335693] rproc_fw_boot 1171
[ 162.379086] rproc_fw_boot 1182
[ 162.382185] rproc_fw_boot 1197
[ 162.385259] rproc_fw_boot 1207
[ 162.389076] omap-rproc 55020000.ipu: deassert_hardreset
[ 162.397632] in 0 0 1 700 210 214
[ 162.400878] stat 7
[ 162.402899] in1 0 0 1 700 210 214
[ 162.422695] stat 6
[ 162.424714] out 0 0 1 700 210 214
[ 162.428041] omap_hwmod: ipu2: failed to hardreset
[ 162.436706] omap_rproc_device_enable: failed for proc 55020000.ipu
[ 162.442969] omap-rproc 55020000.ipu: omap_device_enable failed: -16
[ 162.449371] remoteproc remoteproc1: can't start rproc 55020000.ipu: -16
[ 162.458996] omap-iommu 55082000.mmu: iommu fault: da 0x0 flags 0x0
[ 162.465208] remoteproc remoteproc1: crash detected in 55020000.ipu: type mmufault
[ 162.472728] omap-iommu 55082000.mmu: 55082000.mmu: errs:0x00000002 da:0x00000000 pgd:0xeca44000 *pgd:px00000000
I found a topic in the community have the same issue,but no more reply.