Part Number: TMS320C5534
Tool/software: TI-RTOS
Hello,
My app is using a C55x and the development envSV7, Linux, DSP/BIOS 5.42. As am Linux, the graphical gconf utility is not available :( so i am editing manually
my .tcf file. The problem is, there are quite a lot of things that are available as "checkbox options" in gconf and juts unvailable in Linux, for example
the CLK manager (i discovered it the hard way ...). So, is there a file which i could manually alter and would replace what gconf is doing ?RAM is too small
and I have to manually edit the generated .cmd each time I am re-building from scratch the project.
Is there a way to specify (like in the gconf config panel) that the C secitions should go to SARAM instead ?
Thanks
Jacques