This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Simulator cycle count vs actual hardware cycle count

Part Number: TMS320C6748

Dear Friends,

We are running some algorithm on the "cycle accurate simulator" and on real LCDK target at 456MHZ.

The cycle count on the target board is roughly twice as much as on the simulator.

We have maximum L1 and L2 open (256K).

Any suggestions why this can occur?

Thanks,

Avi Tal

  • Can you share which SDK are you running on the LCDK? Or is this a custom bare metal algorithm?

    Best Regards,
    Yordan
  • Dear Yordan,

    Thanks allot for your answer.

    We are running bare-metal algorithm.

    We are also aware that the simulator assumes zero-wait-state memory and does not simulate L2/DDR latency, so we are not surprised by the results.

    We just want to make sure there is nothing else we are missing.

    Thanks,

    Avi Tal

  • Yes, the additional latency is expected but I am little surprised that the latency is twice of values observed on the simulator. Are you measuring performance using TSCH/TSCL registers?

    Can you confirm L1 Cache is enabled and all your data and code is in L2 ? Also make sure that your data buffers are aligned to cache line boundary.