Part Number: AM5728
Tool/software: Linux
Hi - I recently encountered this known issue (Perl in linux-devkit of the 4.1/4.2 SDK release packages are not relocatable) when building under Processor SDK for Linux:
Can't locate strict.pm in @INC (you may need to install the strict module) (@INC contains: //usr/lib/perl/site_perl/5.22.1 //usr/lib/perl/vendor_perl/5.22.1 //usr/lib/perl/5.22.1 /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/site_perl/5.22.1/ /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/site_perl/5.22.1 /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/vendor_perl/5.22.1/ /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/vendor_perl/5.22.1 /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/5.22.1/ /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/5.22.1 /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/perl/5.22.1 .) at ./lib/build_OID_registry line 14.
BEGIN failed--compilation aborted at ./lib/build_OID_registry line 14.
lib/Makefile:220: recipe for target 'lib/oid_registry_data.c' failed
make[2]: *** [lib/oid_registry_data.c] Error 2
make[2]: *** Waiting for unfinished jobs....
I implemented this workaround:
make ARCH=arm CROSS_COMPILE=../../linux-devkit/sysroot/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- zImage" (or even the full path to arm-linux-gnueabihf-)
Now I can build the kernel out but if I try to build ti-ipc-linux I get the following error:
make ARCH=arm CROSS_COMPILE=~/ti-processor-sdk-linux-am57xx-evm-04.01.00.06/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- ti-ipc-linux
or
make ARCH=arm CROSS_COMPILE=../../linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- ti-ipc-linux
libtool: compile: arm-linux-gnueabihf-gcc "-DPACKAGE_NAME=\"TI IPC\"" -DPACKAGE_TARNAME=\"ti-ipc\" -DPACKAGE_VERSION=\"3.0.0\" "-DPACKAGE_STRING=\"TI IPC 3.0.0\"" -DPACKAGE_BUGREPORT=\"\" -DPACKAGE_URL=\"\" -DPACKAGE=\"ti-ipc\" -DVERSION=\"3.0.0\" -DSTDC_HEADERS=1 -DHAVE_SYS_TYPES_H=1 -DHAVE_SYS_STAT_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_MEMORY_H=1 -DHAVE_STRINGS_H=1 -DHAVE_INTTYPES_H=1 -DHAVE_STDINT_H=1 -DHAVE_UNISTD_H=1 -DHAVE_DLFCN_H=1 -DLT_OBJDIR=\".libs/\" -DSTDC_HEADERS=1 -DHAVE_FCNTL_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_SYS_PARAM_H=1 -DHAVE_SYS_SOCKET_H=1 -DHAVE_SYS_TIME_H=1 -DHAVE_UNISTD_H=1 -I. -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard --sysroot=/home/dmurphy/ti-processor-sdk-linux-am57xx-evm-04.01.00.06/linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi -I../../../hlos_common/include -D_GNU_SOURCE -Wall -I../../../linux/include -I../../../packages -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard --sysroot=/home/dmurphy/ti-processor-sdk-linux-am57xx-evm-04.01.00.06/linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi -MT LAD_client.lo -MD -MP -MF .deps/LAD_client.Tpo -c LAD_client.c -fPIC -DPIC -o .libs/LAD_client.o
../../../libtool: line 1111: arm-linux-gnueabihf-gcc: command not found
Just to confirm, I have also removed the compiler path from $PATH as per the workaround.
dmurphy@tibuilder:~/ti-processor-sdk-linux-am57xx-evm-04.01.00.06$ echo $PATH
/usr/local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games
Any help or recommendation would be much appreciated!
Thanks,
Dermot