Other Parts Discussed in Thread: AM1806, AM1808
Hi,
We are having problems booting a custom made XAM1808 card with the following specifications:
- LAN8710A-EZK-TR, LAN IC
- M25P64-VME6TG, SPI FLASH
- MT46H32M16LFBF, DDR Ram
- NAND01GW3B2CZA6E, NAND Flash
The voltage supplies are made with different circuits according to TI examples.
This is what we know:
- The voltages are correct.
- The oscillator is working at 24Mhz.
- The boot config is set to boot from SPI1 (00001100)
- The SPI Memory is working (verified with a LogicPD card)
- ICs are mounted the correct way.
- RESET_OUT works according to the specifications.
The problems we see:
- No activity on SPI clock line or SPI CS.
- No activity on UART1 or UART2 when changing boot pins accordingly.
Do you have any good ideas where to look for the problem next?
Best Regards,
Niclas