Other Parts Discussed in Thread: OMAPL138
Hi,
I try to run an example of enet_echo from OMAPL138_StarterWare_1_10_04_01 \ examples \ evmOMAPL138 on ARM core.
if(ipMode != IPADDR_USE_STATIC)
{
/* wait till the dynamic IP address is properly assigned */
state = &(sitaraNetIF[instNum].dhcp->state);
while((*state != DHCP_BOUND) && (cnt--));
// *state = 0x0A;
if(0 == cnt)
{
return 0;
}
}
The code is working fine for the first time only ,it can allocate an IP address for my EVM board.when i terminate the debug session and debug it again the code got stuck in while((*state != DHCP_BOUND) && (cnt--)); line..what might be the problem???But if i power off the board and again power ON and debug , it will work fine for the first time only.The problem starts when i terminate debug session and debug it again.
what might be the reason???How to solve it??
I tried to run by connecting the board to our corporate network via ethernet cable.
Regards,
Arun Kumar