My customer is asking what the best case (minimum) latency is from a digital parallel input to the output of the LCD controller. Assuming no processing at this time. Best case scenario. Is this documented somewhere? Thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer is asking what the best case (minimum) latency is from a digital parallel input to the output of the LCD controller. Assuming no processing at this time. Best case scenario. Is this documented somewhere? Thanks!!
Andy,
This is a difficult question to answer since it depends on so many factors.
Best case is close to zero. In order to achieve this though the system would need to use a single frame buffer and have the input source synchronized with the display output.
Worst case could be many frames of delay.
What is the application? Is there a specific input source in mind? What additional processing is required on the image data? Is the plan to use the Linux V4L2 framework etc...?
BR,
Steve
Thank you Steve for such a quick response.
I have answers to your questions, I just can't answer them in an open forum like this. If you are willing, please email me at andy.chernock@avnet.com and I will respond with a description of the application and answers to your questions.
Thank you again!
-ANDY