So, I believe that our team has figured out where we need to start. We created a new CCS project using the C6000 project type, the Generic C64x+ Device with RTSC support, then using the evmDM6467 platform. If this is correct please let us know and then where we need to go from there as we are not sure, we believe we have an idea and are trying it but are not 100% sure. Thanks in advance.