Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: McASP interrupt configuration

Part Number: AM5728

Tool/software: TI-RTOS

Hi,I want to configuer mcasp interrupt method.

1.I configuer    McASP2_IRQ_AXEVT   to   MPU_IRQ_112

CSL_xbarMpuIrqConfigure(CSL_XBAR_INST_MPU_IRQ_112, CSL_XBAR_McASP2_IRQ_AXEVT);

2.But I don't konw how to configuer mcasp interrupt fuction and use interrupt fuction.

Can you give me some help?  Is there a example of  the interrupt ?

  • The RTOS team have been notified. They will respond here.
  • Refer to audio_evmInit.c file in the path pdk_am57xx_1_0_9\packages\ti\drv\mcasp\example\evmDRA7xx\src\dra75x for example of configuring crossbar for connecting MCASP interrupt with MPU IRQ.

    As I mentioned on the other thread most of the example for MCASP in the Processor SDK RTOS are using MCASP LLD driver. DRA7xx and AM57xx examples are mostly using MCASP with EDMA rather than in CPU interrupt mode. Other than the MCASP examples under pdk_am57xx_1_0_9\packages\ti\drv\mcasp\example, the only other example is the example available at pdk_am57xx_1_0_9\packages\ti\csl\example\mcasp but that example is not setting up XBAR for MPU IRQ

    Hope this helps.

    Regards,
    Rahul