Other Parts Discussed in Thread: TMS320DM6467
Hi all!
I'm trying to establish a Linux OS on a DM6467. I have the TMS320DM6467 EVM as a reference board. I flashed the u-boot and uImage properly on the EVM board and it works fine. When I tried to flash the Linux on our board the phy won't work. I asked the board designer and he said that the phy area is copied from the TI board schemes, so it should work the same.
When I command 'ip=off' in the boot environment the Linux rise properly, but doesn't ping. I used the NAND flashing because otherwise the kernel won't download the NFS, so I flashed the RAMDISK to the NAND. The EVM worked properly with the DHCP, but I wanted to do the same process in order to find the difference.
My questions are:
-
what is the phy driver? I'm using the LSI ET1011 phy as in the EVM but there isn't such en option in the kernel configurations. I added som kprints to find what driver it enters, but in the added log file you can see that it enters three different drivers.
-
Can it be a hardware fault? If so, how can I find it?
-
Before I flashed the NAND the uboot downloaded the kernel via Ethernet but the kernel couldn't download the NFS. What's the difference between the uboot end kernel, are they using different drivers?
Thanks a lot
Ely
Here is the log-file when I allow Ethernet:
Starting NAND Copy
Booting Application @ 0x81080000
U-Boot 2009.08 (Sep 05 2010 - 18:58:01)
I2C: ready
DRAM: 256 MB
NAND: 128 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 363MHz
DDR Clock :- 363MHz
Net: Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 3 \0x08\0x08\0x08 2 \0x08\0x08\0x08 1 \0x08\0x08\0x08 0
NAND read: device 0 offset 0x560000, size 0x500000
5242880 bytes read: OK
Loading from NAND 128MiB 3,3V 8-bit, offset 0x160000
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2051748 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2051748 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux..................................................................................................................................... done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@rd3.linux4biz.lan) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Tue Sep 14 12:16:27 IST 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6467 variant 0x1
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 30720
Kernel command line: console=ttyS0,115200n8 root=/dev/ram rw initrd=0x81100000,16M mem=120M
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 100992KB available (3465K code, 697K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (no cpio magic); looks like an initrd
Freeing initrd memory: 16384K
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
=================>>>>>>>>>>>>>> phy_init
=================>>>>>>>>>>>>>> phy_driver_register
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Sep 14 2010 12:19:27 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
=================>>>>>>>>>>>>>>ltt_facilities_init
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
CIR device registered successfully (Major = 252, Minor = 0)
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a ST16654
serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a ST16650V2
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ42): -28
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
=================>>>>>>>>>>>>>> marvell_init
=================>>>>>>>>>>>>>> phy_driver_register
Marvell 88E1101: Registered new driver
=================>>>>>>>>>>>>>> phy_driver_register
Davicom DM9161E: Registered new driver
=================>>>>>>>>>>>>>> phy_driver_register
Davicom DM9131: Registered new driver
=================>>>>>>>>>>>>>> phy_driver_register
SMSC LAN83C185: Registered new driver
=================>>>>>>>>>>>>>> phy_driver_register
Fixed PHY: Registered new driver
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
#0: DaVinci DM6467 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP and RARP requests ...... timed out!
IP-Config: Reopening network devices...
Sending DHCP and RARP requests ...... timed out!
IP-Config: Reopening network devices...
Sending DHCP and RARP requests .....