Part Number: AM5718
Tool/software: Linux
Hi
I am trying the usb boot mode using the micro usb (J45) connected to usb storage device.
the storage device is created with two partitions boot and rootfs and copied the respective files and file system.
But when I go throw the uboot code it is clear that no usb boot mode is enable for am571x.
The changes added by referring am43xx,
In the am57xx_evm.h added #define CONFIG_SYS_USB_FAT_BOOT_PARTITION 1
In am57xx/board.c, added ti_usb_phy_uboot_init(&usb_phy1_device);
Enabled the config SPL / TPL ---> Support USB host drivers -> Support loading from USB
Error:
undefined reference to `ti_usb_phy_uboot_init'
undefined reference to `dwc3_omap_uboot_init'
undefined reference to `dwc3_uboot_init'
undefined reference to `dwc3_uboot_exit'
undefined reference to `dwc3_omap_uboot_exit'
Using the ti-processor-sdk-linux-am57xx-evm-04.01.00.06-Linux-x86-Install.bin
Can you please help us on how to enable the usb boot mode in am571x idk?
Thanks
Mahesh Muni