Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hello,
we activated the 'Fully Preemptible Kernel (RT)' mode in our linux config and have now the issue that the process [ksoftirqd/0] has always high CPU load and blocks the system.
We use the Linux USB Gadget functionality and the problem is more reproducable when a USB connection is available.
Our System:
CPU: TI AM335X
repository: git://git.ti.com/processor-sdk/processor-sdk-linux.git
branch: processor-sdk-linux-rt-03.03.00
Do you know some problems with the preembtion and the ksoftirqd/0?
What can be the cause, that the ksoftirqd/0 has a high cpu load?
Thanks in advance
Regards,
Christian Fisahn