Other Parts Discussed in Thread: AM3517
Can am3517 drive 4 8-bit ddr2 sdram?
We use 4 8-bit ddr2 sdram, but many errors when I test memory.
Below is the mtest commands output from u-boot:
Mem error @ 0x85BCB200: found 5555AA55, expected 55555555
Mem error @ 0x85BF0200: found 5555AA55, expected 55555555
Mem error @ 0x87B7C200: found 5555AA55, expected 55555555
Mem error @ 0x87BEB200: found 5555AA55, expected 55555555
Mem error @ 0x87DD8100: found 5555AA55, expected 55555555
Mem error @ 0x87DF8100: found 5555AA55, expected 55555555
Mem error @ 0x8DB03200: found 5555AA55, expected 55555555
It seems the second chip goes wrong, but it works most time. And other boards have the same error.
I am not sure whether am3517 can drive 4 DDR2 chips.