This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CCSTUDIO-KEYSTONE
Hi,
I am using tci6638k2k processor in our custom board. There are two ports: port 0 (interface eth0) is connected to a PHY and we are using link-interface as MAC-PHY (mode 1). This is working fine.
The other port (port 1) is connected to an FPGA device using SGMII. We are trying to use MAC_MAC_AUTONEG (mode 0) as link-interface for this port. However, this is not working when the FPGA device gets ready. (This port works fine under MAC_MAC_FORCED (mode 2) if FPGA device is already loaded.)
Wondering if this is a known/resolved issue ? (When was it resolved?)
Thanks,
Best Regards,
Nilesh
Hi Yordan,
Thanks for your help! Really appreciate!
We are using ti-processor-sdk-linux-rt-k2hk-evm-03.03.00.04 (based on kernel 4.4.41-rt52).
Thanks again,
Best Regards,
Nilesh
Hi Yordan,
We are using ti-processor-sdk-linux-rt-k2hk-evm-03.03.00.04 (based on kernel 4.4.41-rt52).
When the FPGA device comes up under this config, the link is not getting autonegotiated. Could you please let me know if I am missing anything in using MAC_MAC_AUTONEG?
Thanks!
Best Regards,
Nilesh