Part Number: TDA2
Hello everyone:
Here are my environment:
Hardware:
1. TDA2xx EVM
2. TDA2xx Vision Application Board
3. 6 channel FPD-Link III FMC Daughter Board
4. 2 x OV10635 Sensor
SDK: Vision SDK 3.0.2
I can run use case "vip_single_cam_sgx_display" with single OV10635 connected to P1.
Now, I'm trying to run use case "lvds_vip_multi_cam_view_sgx_display". BUT when I'm using daughter board that two OV10635 camera connected to, the kernel stop at "[ OK ] Started Synchronize System and HW clocks." and then reboot again and agin. I try to remove one of the camera and there is no problem at all. And I also try to use Automotive SDK, the result is the same.
My question is "Can I use only two cameras? How can I do that?"
Thanks in advance