Hello,
Can you explain more specifically what will happen if the sysboot [5:0] are NOT set to one of the settings mentioned on the TRM Table 29-9.
specifically what will be the behavior if they are all ones or all zeros.
Thanks
Guy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you explain more specifically what will happen if the sysboot [5:0] are NOT set to one of the settings mentioned on the TRM Table 29-9.
specifically what will be the behavior if they are all ones or all zeros.
Thanks
Guy
Hi Guy,
sysboot[5:0] = 000000 - Is a supported combination USB --> eMMC
sysboot[5:0] = 111111 - Is reserved unless you are using an emulation device (a TDA2x type)
Combinations not listed in table 29-9 should be considered reserved, i.e. boot will not happen.
Please make sure you have the latest TRM - there was updates some months ago.
Regards,
Stan