Other Parts Discussed in Thread: TVP5158
Hi,
Currently I am considering of using DM365 for my project that require video processing of 4 D1 channel into H.264 for my DVR application. However, from the reference design it can only support for up to maximum 2 channel of D1. In this case, my option would be using 2 DM365. However, I do not sure how 2 DM365 IC can be use along with a single hard disk drive. Currently is there any technology/ways that can implement this.