This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDXIDK5718: Boot timing and reporting

Part Number: TMDXIDK5718
Other Parts Discussed in Thread: AM5718

Tool/software: Linux

Hi 

I'm using TI SDK with u-boot-2017.01+gitAUTOINC+c68ed086bd-gc68ed086bd.

I enabled Boot timing:

On the console I see the following:

Issue 1): Why is the output partly clobbered?

After linux is started I dumped the "bootstage" part of the devicetree into a file:

find /proc/device-tree/bootstage/ -type f -exec head {} + | less >bootstage.txt

Below the file.

Issue 2)

Can you explain what is the meaning of the node name  (e.g. 45) and the mark attribute (e.g. id=15).

As an example I see "bootstage_mark_name(BOOTSTAGE_ID_MAIN_LOOP, "main_loop"); in the code. but in the tree I see object name 44. BOOTSTAGE_ID_MAIN_LOOP is defined as 171.

Regards, Chris