Part Number: AM3354
Tool/software: Linux
Hi
we are using AM3354 + processor SDK 03.02.00.05 with kernel 4.4.32.
originally we are using the nand flash chip Spansion S34ML08G101TF100
the spec is 1GB capacity.2k page.128k block and 512 sub-page size.
We are using BCH8 ECC for both uboot and kernel.And we are using UBIFS as it's the default choice from the processor SDK.
And it works fine.
Right now i need to switch to another nand flash chip with the model Samsung K9K8G08U0E.
From the spec it seems basically identical to the spansion chip.Same capacity.Same page/block/sub-page size and all.
So i figured that maybe i won't need to change any code to get this chip working?
When i boot up the kernel with this samsung chip for the 1st time.It looks ok. But after a reboot. There are these ECC errors printed when kernel is booting up.
Like this:
omap-gpmc 50000000.gpmc: GPMC revision 6.0
gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
nand: device found, Manufacturer ID: 0xec, Chip ID: 0xd3
nand: Samsung NAND 1GiB 3,3V 8-bit
nand: 1024 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
9 ofpart partitions found on MTD device 8000000.nand
Creating 9 MTD partitions on "8000000.nand":
0x000000000000-0x000000020000 : "NAND.SPL"
0x000000020000-0x000000040000 : "NAND.SPL.backup1"
0x000000040000-0x000000060000 : "NAND.SPL.backup2"
0x000000060000-0x000000080000 : "NAND.SPL.backup3"
0x000000080000-0x000000260000 : "NAND.u-boot"
0x000000260000-0x000000280000 : "NAND.u-boot-env"
0x000000280000-0x000000580000 : "NAND.LOGO"
0x000000580000-0x000000a80000 : "NAND.kernel"
0x000000a80000-0x000040000000 : "rootfs"
ubi0: attaching mtd8
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 1885:0, read only 64 bytes, retry
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
omap2-nand 8000000.nand: uncorrectable bit-flips found
ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 1885:0, read only 64 bytes, retry
I'm attaching both the specs of the nand chips.And my dts file.
2553.k9k8g08u0e-sib0.pdf7343.S34ML08G1.pdf
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "am33xx.dtsi"
#include <dt-bindings/interrupt-controller/irq.h>
#include <dt-bindings/gpio/gpio.h>
/ {
model = "TI AM335x EVM";
compatible = "ti,am335x-evm", "ti,am33xx";
cpus {
cpu@0 {
cpu0-supply = <&vdd1_reg>;
};
};
memory {
device_type = "memory";
reg = <0x80000000 0x20000000>; /* 512 MB */
};
vbat: fixedregulator@0 {
compatible = "regulator-fixed";
regulator-name = "vbat";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-boot-on;
};
lis3_reg: fixedregulator@1 {
compatible = "regulator-fixed";
regulator-name = "lis3_reg";
regulator-boot-on;
};
wlan_en_reg: fixedregulator@2 {
compatible = "regulator-fixed";
regulator-name = "wlan-en-regulator";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
/* WLAN_EN GPIO for this board - Bank1, pin16 */
gpio = <&gpio1 16 0>;
/* WLAN card specific delay */
startup-delay-us = <70000>;
enable-active-high;
};
backlight {
compatible = "pwm-backlight";
pwms = <&ehrpwm1 1 50000 0>;
brightness-levels = <0 51 53 56 62 75 101 152 255>;
default-brightness-level = <8>;
};
panel {
compatible = "ti,tilcdc,panel";
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&lcd_pins_s0>;
panel-info {
ac-bias = <255>;
ac-bias-intrpt = <0>;
dma-burst-sz = <16>;
bpp = <32>;
fdd = <0x80>;
sync-edge = <0>;
sync-ctrl = <1>;
raster-order = <0>;
fifo-th = <0>;
};
display-timings {
800x480p62 {
clock-frequency = <30000000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <40>;
hback-porch = <88>;
hsync-len = <48>;
vback-porch = <32>;
vfront-porch = <13>;
vsync-len = <3>;
hsync-active = <1>;
vsync-active = <1>;
pixelclk-active = <0>;
};
};
};
leds {
pinctrl-names = "default";
pinctrl-0 = <&user_leds_default>;
compatible = "gpio-leds";
usb1_5v_power {
label = "usb1_5v_power";
gpios = <&gpio3 13 GPIO_ACTIVE_LOW>;
default-state = "on";
};
};
};
/*
* pin number = value in "AM335x Technical Reference Manual Table 9-10. CONTROL_MODULE REGISTERS" - 0x800
*/
&am33xx_pinmux {
pinctrl-names = "default";
pinctrl-0 = <&clkout2_pin>;
i2c0_pins: pinmux_i2c0_pins {
pinctrl-single,pins = <
0x188 (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_sda.i2c0_sda */
0x18c (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_scl.i2c0_scl */
>;
};
i2c1_pins: pinmux_i2c1_pins {
pinctrl-single,pins = <
0x180 (PIN_INPUT_PULLUP | MUX_MODE3) /* uart1_rxd.i2c1_sda */
0x184 (PIN_INPUT_PULLUP | MUX_MODE3) /* uart1_txd.i2c1_scl */
>;
};
touchscreen_pins: pinmux_touchscreen_pins {
pinctrl-single,pins = <
0x54 (PIN_OUTPUT | MUX_MODE7) /* gpmc_a5.gpio1_21 GPIO1_21_TCH_RST */
0x50 (PIN_INPUT | MUX_MODE7) /* gpmc_a4.gpio1_20 GPIO1_20_TCH_INT */
>;
};
uart0_pins: pinmux_uart0_pins {
pinctrl-single,pins = <
0x170 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
0x174 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
>;
};
clkout2_pin: pinmux_clkout2_pin {
pinctrl-single,pins = <
0x1b4 (PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* xdma_event_intr1.clkout2 */
>;
};
nandflash_pins_s0: nandflash_pins_s0 {
pinctrl-single,pins = <
0x0 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad0.gpmc_ad0 */
0x4 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad1.gpmc_ad1 */
0x8 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad2.gpmc_ad2 */
0xc (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad3.gpmc_ad3 */
0x10 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad4.gpmc_ad4 */
0x14 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad5.gpmc_ad5 */
0x18 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad6.gpmc_ad6 */
0x1c (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad7.gpmc_ad7 */
0x70 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_wait0.gpmc_wait0 */
0x74 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_wpn.gpmc_wpn */
0x7c (PIN_OUTPUT | MUX_MODE0) /* gpmc_csn0.gpmc_csn0 */
0x90 (PIN_OUTPUT | MUX_MODE0) /* gpmc_advn_ale.gpmc_advn_ale */
0x94 (PIN_OUTPUT | MUX_MODE0) /* gpmc_oen_ren.gpmc_oen_ren */
0x98 (PIN_OUTPUT | MUX_MODE0) /* gpmc_wen.gpmc_wen */
0x9c (PIN_OUTPUT | MUX_MODE0) /* gpmc_be0n_cle.gpmc_be0n_cle */
>;
};
cpsw_default: cpsw_default {
pinctrl-single,pins = <
0x144 (PIN_INPUT_PULLDOWN | MUX_MODE0) /* RMII1_REFCLK */
0x124 (PIN_OUTPUT | MUX_MODE1) /* RMII1_TXD1 */
0x128 (PIN_OUTPUT | MUX_MODE1) /* RMII1_TXD0 */
0x114 (PIN_OUTPUT | MUX_MODE1) /* RMII1_TXEN */
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE1) /* RMII1_RXD1 */
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* RMII1_RXD0 */
0x10c (PIN_INPUT_PULLDOWN | MUX_MODE1) /* RMII1_CRS_DV */
0x110 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* RMII1_RXERR */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
0x144 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_REFCLK */
0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_TXD1 */
0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_TXD0 */
0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_TXEN */
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_RXD1 */
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_RXD0 */
0x10c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_CRS_DV */
0x110 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* RMII1_RXERR */
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
mmc1_pins: pinmux_mmc1_pins {
pinctrl-single,pins = <
0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
lcd_pins_s0: lcd_pins_s0 {
pinctrl-single,pins = <
0x20 0x01 /* gpmc_ad8.lcd_data16, OUTPUT | MODE1 */
0x24 0x01 /* gpmc_ad9.lcd_data17, OUTPUT | MODE1 */
0xa0 0x00 /* lcd_data0.lcd_data0, OUTPUT | MODE0 */
0xa4 0x00 /* lcd_data1.lcd_data1, OUTPUT | MODE0 */
0xa8 0x00 /* lcd_data2.lcd_data2, OUTPUT | MODE0 */
0xac 0x00 /* lcd_data3.lcd_data3, OUTPUT | MODE0 */
0xb0 0x00 /* lcd_data4.lcd_data4, OUTPUT | MODE0 */
0xb4 0x00 /* lcd_data5.lcd_data5, OUTPUT | MODE0 */
0xb8 0x00 /* lcd_data6.lcd_data6, OUTPUT | MODE0 */
0xbc 0x00 /* lcd_data7.lcd_data7, OUTPUT | MODE0 */
0xc0 0x00 /* lcd_data8.lcd_data8, OUTPUT | MODE0 */
0xc4 0x00 /* lcd_data9.lcd_data9, OUTPUT | MODE0 */
0xc8 0x00 /* lcd_data10.lcd_data10, OUTPUT | MODE0 */
0xcc 0x00 /* lcd_data11.lcd_data11, OUTPUT | MODE0 */
0xd0 0x00 /* lcd_data12.lcd_data12, OUTPUT | MODE0 */
0xd4 0x00 /* lcd_data13.lcd_data13, OUTPUT | MODE0 */
0xd8 0x00 /* lcd_data14.lcd_data14, OUTPUT | MODE0 */
0xdc 0x00 /* lcd_data15.lcd_data15, OUTPUT | MODE0 */
0xe0 0x00 /* lcd_vsync.lcd_vsync, OUTPUT | MODE0 */
0xe4 0x00 /* lcd_hsync.lcd_hsync, OUTPUT | MODE0 */
0xe8 0x00 /* lcd_pclk.lcd_pclk, OUTPUT | MODE0 */
0xec 0x00 /* lcd_ac_bias_en.lcd_ac_bias_en, OUTPUT | MODE0 */
>;
};
ehrpwm1_pins_default: backlight_pins {
pinctrl-single,pins = <
0x4c (PIN_OUTPUT | MUX_MODE6) /* GPIO1_19_LCD_PWM_1B gpmc_a3=ehrpwm1B_mux1 MODE6 */
>;
};
user_leds_default: user_leds_default {
pinctrl-single,pins = <
0x234 (PIN_OUTPUT | MUX_MODE7) /* conf_usb1_drvvbus.gpio3_13 GPIO3_13_USB1_POWER */
>;
};
};
&uart0 {
pinctrl-names = "default";
pinctrl-0 = <&uart0_pins>;
status = "okay";
};
&i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
status = "okay";
clock-frequency = <400000>;
tps: tps@2d {
reg = <0x2d>;
};
};
&i2c1 {
pinctrl-names = "default";
pinctrl-0 = <&i2c1_pins>;
status = "okay";
clock-frequency = <400000>;
gt911a: gt911a@5d {
compatible = "goodix,gt911a";
pinctrl-names = "default";
pinctrl-0 = <&touchscreen_pins>;
reg = <0x5d>;
interrupt-parent = <&gpio1>;
interrupts = <20 2>;
reset-gpios = <&gpio1 21 0>;
int-gpios = <&gpio1 20 0>;
};
};
&usb {
status = "okay";
};
&usb_ctrl_mod {
status = "okay";
};
&usb0_phy {
status = "okay";
};
&usb1_phy {
status = "okay";
};
&usb0 {
status = "okay";
};
&usb1 {
status = "okay";
dr_mode = "host";
};
&cppi41dma {
status = "okay";
};
&lcdc {
status = "okay";
blue-and-red-wiring = "crossed";
};
&elm {
status = "okay";
};
&epwmss1 {
status = "okay";
ehrpwm1: pwm@48302200 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&ehrpwm1_pins_default>;
};
};
&gpmc {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&nandflash_pins_s0>;
ranges = <0 0 0x08000000 0x20000000>; /* CS0: NAND */
nand@0,0 {
compatible = "ti,omap2-nand";
reg = <0 0 4>; /* CS0, offset 0, IO size 4 */
interrupt-parent = <&gpmc>;
interrupts = <0 IRQ_TYPE_NONE>, /* fifoevent */
<1 IRQ_TYPE_NONE>; /* termcount */
rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <44>;
gpmc,cs-wr-off-ns = <44>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <34>;
gpmc,adv-wr-off-ns = <44>;
gpmc,we-on-ns = <0>;
gpmc,we-off-ns = <40>;
gpmc,oe-on-ns = <0>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <64>;
gpmc,rd-cycle-ns = <82>;
gpmc,wr-cycle-ns = <82>;
gpmc,wait-on-read = "true";
gpmc,wait-on-write = "true";
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wait-monitoring-ns = <0>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
read-only;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
read-only;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
read-only;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
read-only;
};
partition@4 {
label = "NAND.u-boot";
reg = <0x00080000 0x001E0000>;
read-only;
};
partition@5 {
label = "NAND.u-boot-env";
reg = <0x00260000 0x00020000>;
read-only;
};
partition@6 {
label = "NAND.LOGO";
reg = <0x00280000 0x00300000>;
read-only;
};
partition@7 {
label = "NAND.kernel";
reg = <0x00580000 0x00500000>;
read-only;
};
partition@8 {
label = "rootfs";
reg = <0x00A80000 0x3F580000>;
};
};
};
#include "tps65910.dtsi"
&tps {
vcc1-supply = <&vbat>;
vcc2-supply = <&vbat>;
vcc3-supply = <&vbat>;
vcc4-supply = <&vbat>;
vcc5-supply = <&vbat>;
vcc6-supply = <&vbat>;
vcc7-supply = <&vbat>;
vccio-supply = <&vbat>;
regulators {
vrtc_reg: regulator@0 {
regulator-always-on;
};
vio_reg: regulator@1 {
regulator-always-on;
};
vdd1_reg: regulator@2 {
/* VDD_MPU voltage limits 0.95V - 1.26V with +/-4% tolerance */
regulator-name = "vdd_mpu";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1351500>;
regulator-boot-on;
regulator-always-on;
};
vdd2_reg: regulator@3 {
/* VDD_CORE voltage limits 0.95V - 1.1V with +/-4% tolerance */
regulator-name = "vdd_core";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1150000>;
regulator-boot-on;
regulator-always-on;
};
vdd3_reg: regulator@4 {
regulator-always-on;
};
vdig1_reg: regulator@5 {
regulator-always-on;
};
vdig2_reg: regulator@6 {
regulator-always-on;
};
vpll_reg: regulator@7 {
regulator-always-on;
};
vdac_reg: regulator@8 {
regulator-always-on;
};
vaux1_reg: regulator@9 {
regulator-always-on;
};
vaux2_reg: regulator@10 {
regulator-always-on;
};
vaux33_reg: regulator@11 {
regulator-always-on;
};
vmmc_reg: regulator@12 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
};
&mac {
slaves = <1>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rmii";
};
&phy_sel {
rmii-clock-ext;
};
&mmc1 {
status = "okay";
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc1_pins>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_LOW>;
};
&sham {
status = "disabled";
};
&aes {
status = "disabled";
};
&rng {
status = "disabled";
};
&wkup_m3_ipc {
ti,scale-data-fw = "am335x-evm-scale-data.bin";
};
&sgx {
status = "okay";
};
Could you help me identify what could possibly be the cause?
thanks guys.
yandong