Part Number: AM5728
Tool/software: Linux
Hi TI,
When I try to do boot from mSATA,
I observed, After power on the board(AM5728 evm) nothing is displaying on the GTKterm.
H/W selection:
1. Sata selection J1 connected
2. Boot from sata, jumper settings: J3(1-2), J4(2-3),J5(2-3).
3. short J5
4. disk info:
fdisk -l /dev/sda
Disk /dev/sda: 29.5 GiB, 31671156224 bytes, 61857727 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x1eb46c48
Device Boot Start End Sectors Size Id Type
/dev/sda1 * 2048 1050623 1048576 512M c W95 FAT32 (LBA)
/dev/sda2 1050624 61857726 60807103 29G 83 Linux
5. Copied required images into boot partition:
root@am57xx-evm:/run/media/sda1# ls
MLO u-boot.img uEnv.txt ws-calibrate.rules
The above files copied from working sd images.
Please suggest if am missing anything.
Thanks,
Anil