This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2PXEVM: TDA2PXEVM

Part Number: TDA2PXEVM

Tool/software: TI-RTOS

Hi, 

Built bios all for TDA2p platform using vision SDK 3.02. 

Created a SD card for booting the EVM and I get the following output. The MPU enters retention mode , boot does not proceed and the system is stuck

Tried to use all options of generated MLOs as shown below but the MPU enters retention mode and nothing appears on the screen. 

See listing below. 

PROCESSOR_SDK_VISION_03_02_00_00/vision_sdk$ ls binaries/apps/tda2px_evm_bios_all/sbl/sd/

opp_high opp_low opp_nom opp_od

 

What may be the root cause for that? 

=======================

TDA2Px SBL Boot 

DPLL Configuration Completed 

Clock Domain Configuration Completed 

Module Enable Configuration Completed 

TI EVM PAD Config Completed 

DDR Config Completed 

App Image Download Begins 

SD Boot - file open completed successfully 

MPU CPU0 Image Load Completed 

IPU1 CPU0 Image Load Completed 

IPU1 CPU1 Image Load Completed 

IPU2 CPU0 and CPU1 Image Load Completed 

DSP1 Image Load Completed 

DSP2 Image Load Completed 

EVE1 Image Load Completed 

EVE2 Image Load Completed 

App Image Download Completed 

Putting MPU CPU1 in Off mode 

EVE MMU configuration completed 

EVE MMU configuration completed 

*****************************************************************

PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles 

SBL Initial Config Cycles - 104832  (8.94 ms)
SOC Init Cycles - 170451  (14.54 ms)
DDR Config Clock Cycles - 42953  (3.66 ms)
App Image Load Cycles - 519656  (44.34 ms)
Slave Core Bootup Cycles - 130921  (11.17 ms)
SBL Boot-up Cycles - 969874  (82.76 ms)
Time at which SBL started IPU1_0 - 15257  (1.30 ms)
*****************************************************************

Putting MPU in Retention…

Thanks,

Yair