Part Number: TMS320C5515
Tool/software: Code Composer Studio
Hello,
I inherited a TMS320C5515 project and can't compile it yet because the project paths from the original Code Composer workspace are different than the ones on the computer where it's installed now. I'll resolve those things in time, but before I do I need to flash one of our TMS320 boards to make sure it is functioning. Since I can't build the project yet and then start a debug session to flash the DSP under Code Composer, my question is this: Is there a way for me to flash the previously compiled code into the TMS320 without having to rebuild the project? Using either Code Composer or another standalone program? I'm using an XDS200 debugger with our custom board--same debugger used for the TMS320C5515 EVM.
Thanks for any insight on this.
Best Regards,
Mike McCully