Part Number: DM505
Support Path: /Product/Help with Device Selection/Processor solutions/Digital signal processing devices/
Am want to use DM505L in my design, Please clear the below.
1) In DM505L can i develop by using only DSP with CCS without any RTOS support for ARM. i.e can i develop independently without arm coding to reduce the code complexities if required.
2) If required can i disable ARM Cortex and use only DSP blocks to make the power saving .
3) Can you provide Booting process for DSP .Is it mandatory that first ARM should Boot then DSP.
4) As Development kit available for DM505x.does the kit available separately for DM505L (Single core) to reduce the cost less than DM505M(Dual core).
Please clear the below as soon as you can there by i can able to select the processor for my design.