Part Number: AM5718
Hi champs,
I have a question about "How to calculate for USB3.0 SSC" .
My customer fail USB3.0 TX Compliance test 'TSSC-Freq-Dev-Min and TSSC-Mod-Rate'.
I check at TRM 
P.6852, 26.2.4.3.5 USB3_PHY DPLL Subsystem Architecture.
I think that SSC setting procedure is written in this session.
They want to set as follow.
Frequency deviation 30 k - 33 kHz
Modulation rate
MAX -300 ppm to 300 ppm
MIN -5300 ppm to -3700 ppm
Please tell me specific calculation.
Regards,
Shinji Ueda