Part Number: EVMK2G
Tool/software: TI-RTOS
Hi.
I'm trying to build and run the K2G_bf_rt app of the RTOS SDK.
after a few struggles, i got it to compile, but am getting the following:
"configPkg/linker.cmd", line 31: error #10264: MSMCSRAM memory range overlaps existing memory range MSMC_SRAM
"configPkg/linker.cmd", line 32: error #10264: L2SRAM memory range overlaps existing memory range L2_SRAM_0
"configPkg/linker.cmd", line 32: error #10264: L2SRAM memory range overlaps existing memory range L2_SRAM_1
"configPkg/linker.cmd", line 33: error #10264: EXT_RAM memory range overlaps existing memory range DDR0
warning #10247-D: creating output section ".bferam" without a SECTIONS specification
warning #10247-D: creating output section ".bfiram" without a SECTIONS specification
error #10010: errors encountered during linking; "K2G_bf_rt.out" not built
>> Compilation failure
makefile:168: recipe for target 'K2G_bf_rt.out' failed
gmake: *** [K2G_bf_rt.out] Error 1
gmake: Target 'all' not remade because of errors.
any help would be appreciated,
thank you