Hi,
I am testing the TMDSEVM6678LE by running the supplied code examples. I am using only one core out of 8 that the c6678 has. The problem is: when I execute the hyperlink example, it runs only once. To re-run the code I need to unplug & plug the board. Nothing else helps, Terminate & CPU buttons become useless.
1) What do I have to do in-order to re-run the code?
2) Can I reset one core and keep all the other running?
3) Where can I find a 'timeout' example routine?
4) If the current working core gets stuck, is it possible to trigger another core?
Kind regards
Moti