Part Number: TMS320C5517
Hi,
I'm debugging C5517EVM NOR Flash Boot by using CCSv7.
After boot are completed, I connected to the CCS and I set hardware breakpoint to entrypoint c_int00.
Then pressing hardware reset button on the EVM and press run button via CCS,
C5517 are stopped at c_int00 as expected.
Now, I want to stop the execution at entry of internal ROM bootloader of C5517(which address is 0xFF683C)
after pressing the hardware reset. So, I set the hardware breakpoint at 0xFF683C,
but the program counter always stop at 0xFF7128 when I tried it.
Isn't 0xFF683C the entry point of ROM Bootloader? It seems that bootloader are not executing from 0xFF683C.
best regards,
g.f.