Part Number: AM5728
TRM doc: spruhz6j
Issue 1:
In section "9.4.4.3.3 Input: A:RGB, B:YUV422; Output: A:RGB, B:Scaled YUV420", from Figure 9-8 I can see Y_LO and UV_LO output RGB signals sourced directly from Port A. So I guess VIPx_RGB_OUT_LO_SELECT should equal 1 but it says "VIPx_RGB_OUT_LO_SELECT = 0" in the description of the section.
Issue 2:
In Figure 9-7 of section "9.4.4.3.2 Input: A:YUV422 8/16, B:YUV422; Output: A:Scaled YUV420, B: RGB", I can see the Y_UP and UV_UP output RGB signal sourced from VIP_RGB MUX whose input is the output of VIP_CSC. So "VIPx_RGB_OUT_HI_SELECT = 1" & "VIPx_RGB_SRC_SELECT = 0" are easy to understand. At this time VIP_RGB MUX whose value is determined by (VIPx_RGB_OUT_HI_SELECT, VIPx_RGB_SRC_SELECT) is evaluated as 0b10 but the red line is connecting to "3" of VIP_RGB MUX.
Why?