This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/OMAP-L138: TI v7.4.14

Part Number: OMAP-L138

Tool/software: TI C/C++ Compiler

I am working on OMAP-L138 for audio processing. My code includes FFT, MFCC, and GMM to classify the bird sound. There is no compile error, but it stops when I run the program.

It seems the problem is a memory, because I can see that the memory values change while running the code by seeing the dnuebugging mode. 

Another issue is that I cannot use the dynamic memory allocation (malloc and calloc), therefore, I assigned the memory with arrays only.

Is there any manual to solve the problem?