Part Number: BEAGLEBK
Tool/software: Linux
hello.
* I created me a custom board with the beagle core : http://beaglecore.com/
* i created me a own linux image with buildroot.
* my Wf111 is connected to the mm3 of the sitara mcu.
* in the attachement are several files from my test. You can see following:
** my devicetree in the file"am335x-beagle_core_series3.dtsi" and "am335x-boneblack.dts"
* * result of the wf111_supportinfo_result.sh"
** result of the dsmeg command
** in the pinmux files you can see that the pinmux pin are looking correctly (for my understanding)
** in the "cat_pinmux-pins.txt" you can see that the mmc3 pins are not visible. What is wrong?
**I read this documentation www.silabs.com/.../UG220.pdf.
But I'm stucking on step 2. I dont see this information "new high speed SDIO card at address 0001"
** I read this www.silabs.com/.../AN996.pdf
I have a project that we have to finish asap. We would like to use 2.000-3.000 per year of the wf111 together with the beagle core project
Can you help me please?
wifi_results.zip
thanks a lot!