Part Number: TMDSSK3358
Other Parts Discussed in Thread: PROFIBUS, AM3358
Tool/software: Code Composer Studio
Hi
I'm trying to run the profibus slave PRU example on my Sitara AM3358 Eval Board. What I have done so far:
1: Downloaded the Profibus Slave PRU and installed it (http://software-dl.ti.com/processor-industrial-sw/esd/PRU-ICSS-PROFIBUS-SLAVE/latest/index_FDS.html
2: Changed the paths and version numbers in the "projectCreate.bat" (\ti\PRU-ICSS-Profibus_Slave_01.00.01.01\protocols\profibus_slave\projects)
3: Run the "projectCreate.bat" (Works, gives a note: "Compiler version 'GNU_4.9.3:Linaro' is not currently installed! - defaulting to 'GNU_6.3.1:Linaro'.)
4: Opened the Code Composer Studio and built the example
This gives the error:
/ti/bios_6_52_00_12/packages/ti/sysbios/rts/gnu/ReentSupport.c:83: undefined reference to `ti_sysbios_rts_gnu_ReentSupport_checkIfCorrectLibrary'
Any idea? Could it be something with this Linaro 4.9.3 note?
I'm using Code Composer Studio 8 on Windows, but it gives the same error on Linux.
Thanks!
Corono