Hello,
I use the C6457 chip in the project I'm working on.
I am having trouble with the on-chip BIOS and I am looking for help.
I can change the HWI in the DSP / BIOS Config, and I know that these are prioritized in order.
1. I wonder if it is possible to change the priority of these users as they like.
2. And I wonder how to change it.
3. If it is supposed to be HWI_RESERVED0 OR 1, it is possible to make HWI_INT4 ~ 15 higher priority.
I am currently using CCS 3.3.
Thanks, I Waiting your Help