This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: USB OTG and iOS Support

Part Number: 66AK2G12

Hi,

My customer would like to know if K2G USB has OTG support and if it's iOS compatible?

Thanks,

Chuchen

  • See Section 6.10.19 USB from the device Data Manual & Section 11.19.1.2 Main Features from the TRM:

    The following are USB features which are not supported:
    • USB3.0 SuperSpeed (5Gbps) or USB3.1 SuperSpeed+ (10Gbps) operation in either host or device modes
    • OTG Functionality

    Best Regards,
    Yordan